2/18/2016 2:22 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi AlwintGru, there are 2 transfer-area-types that can be selected in the I-Device-properties. -Application: the Input-Adresses, that you are project in the I-Device are Output-Adresses in the IO-Controller -IO-Transfer area: There you can set a whole module or submodule as transfer area. detailed information about it, you find in this Manual, chapter 4.8: SIMATIC PROFINET System Descriptionhope this helps, regards, |
FCK WAR! |
|
2/22/2016 1:08 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi Alwin, for Communication between two SIMATIC-Controller I always first have a look in this manual: CPU-CPU Communication with SIMATIC ControllersThere you find out every possibility of communication between them. In your case, S7-300 and S7-400, see page 96. I think the easiest way to communicate in this way is to use PUT/GET with S7-Communication. Following FAQ with Applicationsample may help you: How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?hope this helps, regards, |
FCK WAR! |
|
Follow us on