6/10/2024 9:15 AM | |
Joined: 1/4/2007 Last visit: 9/2/2024 Posts: 1142 Rating:
|
Hati is totally right. But I would like to add some more information for you: I don’t recommend to use such an old firmware! The firmware V5.3.4 is more than 15 years old! I recommend you to use the latest firmware V9.5.3. But anyway, let’s take a look together to your error messages to find the issue. You can take a look into the Hardware-config of your Simatic Manager OR (and this is my recommendation): work with the Siwatool software (order-number: 7MH4900-1AK01). Pay attention, that you need also the Siwatool-cable between your computer and the Siwarex FTA module with the order number 7MH4702-8CA. Also, when your computer has no RS232 port, then you need also an USB/RS232-adapter. If so, I recommend you to use the USB/RS232-adapter of the company ATEN, model: UC-232A: https://support.industry.siemens.com/cs/ww/en/view/28391503 Best regards Siwarexi |
Last edited by: Jen_Moderator at: 06/10/2024 12:32:32Text formatting optimized. |
|
Follow us on