8/2/2022 8:35 PM | |
Joined: 12/28/2016 Last visit: 11/12/2024 Posts: 364 Rating:
|
Hi Experts, Please help me with the speed variations , I digged into the parameter file and the drawings of the drive . P741 is set to 11 VDC . On the Tach XT 103 , XT104 input there is a Card which is called Speed calculation Card which is behaving like a tacho i beleive. P083 is selected freely wired , on checking P609 it says K9210 Dont have full idea what is going on here AttachmentSIMOREG DC MASTER.zip (1150 Downloads) |
Last edited by: qwemx at: 08/02/2022 20:40:08With kind regards... |
|
Follow us on