4/10/2022 9:17 AM | |
Joined: 2/12/2021 Last visit: 11/16/2023 Posts: 2 Rating: (0) |
can i ask aquestion I have step7 v5.5+sp4 K5.5.4.0 which micromaster must have because the 5.4 hf2 doesnt much. regards
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 04/11/2022 14:44:41New subject after splitting |
|
4/11/2022 3:10 PM | |
Joined: 9/27/2006 Last visit: 9/24/2024 Posts: 12282 Rating: (2685) |
Hello; Please tell us what problems you have exacly with your drive, and what you would like to do with Step 7 to control the drive, Normally you would use a PLC program to control digital and analog I/O connected to the drive inputs, for example, or to program the exchanges between the drive and the PLC over Profibus-DP. What is your situation? If your question is about Starter software, it works without Step 7, and you can download it here: https://support.industry.siemens.com/cs/ww/en/view/26233208 Hope this helps, Daniel Chartier |
Follow us on