9/16/2021 7:24 AM | |
Joined: 8/25/2006 Last visit: 5/14/2024 Posts: 2205 Rating: (277)
|
Hello. CP1616 does not have FO ports. I think this is ibaFOB-TDC card. There should be at least 2 such cards in iba-PC. You have TDC-Request connection via GDM FO rack coupling. You need to create one more channel with SER04A/SER04B blocks for required CPU, but with different CPU short name at AT/AR inputs of these blocks (PDAnnCMD, nnPDAACK, nnPDADAT). Look at the manual attached. AttachmentibaPDA-Request-SD-TDC_v4.4_en.zip (925 Downloads) |
Follow us on