1/5/2022 12:05 AM | |
Joined: 8/3/2021 Last visit: 6/13/2024 Posts: 120 Rating:
|
HW configuration: - S7 1200 CPU - 1x 16DI/16DQ - 1x 16DI/16DQ (both DIO modules are 6ES7 223-1PL32-0XB0 - FW V2.0) The last modul is connected directly OR connected by bus extension cable (we have tested both variants). Both DI/DQ modules was switched in between during testing. SW configuration: Simple empty project. Only copying clock 0,5Hz to some outputs of DI/DQ modules. The second DI/DQ module always doesn't work (output is not set and inputs don't pass to program although we see inputs LEDs lights when connecting signal to inputs). And its DIAG green LED blinks. Its the same for all four variants (with/without extension cable; switched modules). Project and photo of hardware enclosed. It's weird behaviour and I don't absolutly have any idea whats the problem... AttachmentTest.zip (302 Downloads) |
TIA Portal V13/14/16 |
|
Follow us on