1/21/2015 10:24 AM | |
Joined: 9/23/2005 Last visit: 6/26/2024 Posts: 4347 Rating:
|
Hi, A new feature that STEP7 V13 SP1 brings is the "Undo" in online mode.In older versions, after a download / change to online monitoring, the “undo” button were “disable”. Now, the “undo” feature still available even after online monitoring. Particularly in the commissioning phase, but also in the case of repairs to a running automation plant, small changes are often introduced for testing purposes which are not always successful. For this reason it is important to be able to "Undo" the changes 100% and as fast as possible. This feature is available with V13 SP1, even if an online connection exists between engineering and PLC. TIP: You need to do so many “undo’s” clicks as desired to find the undo “point”. After that you need download the changes to the PLC. Attached there is a cast using this feature. Due upload size limitation, the .AVI was “zipped” in 7z format berore "zipped" in Zip format. Attachmentundo.zip (85 Downloads) |
Last edited by: Min_Moderator at: 1/21/2015 11:59 AMRenamed attachment Denilson Pegaia |
|
Follow us on