8/19/2021 2:47 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
I think you mean with 0BA1 LOGO! the current LOGO! 8.3 (6ED1052-XXX08-0BA1). For this you need the current LSC version 8.3. You can download for free the upgrade to LSC V8.3: Download for LOGO! 8.3 Software UpgradeBut the download is export restricted. Why do you have to log in and register for downloading export-restricted software and what data do you need for this? |
8/19/2021 3:11 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
Sure, your old was a LOGO!8.FS4 in the device selection. Your new LOGO! is a LOGO! 8.3 in the device selection. |
8/19/2021 4:40 PM | |
Joined: 6/24/2010 Last visit: 5/25/2023 Posts: 8 Rating: (0) |
When I want to change the model, I get this message , and the LOGO 8.3 doesn't appear in the list Failed to load panel |
8/19/2021 4:46 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
Are you shure that you have LSC V8.3? |
8/19/2021 4:52 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
Please can you upload the original program from the LOGO!8.2 (6ED1052-XXX08-0BA0) as a zip file? |
8/19/2021 5:02 PM | |
Joined: 6/24/2010 Last visit: 5/25/2023 Posts: 8 Rating: (0) |
The version of LSC is 8.3.0 ( 2020-09-21 11.42) zip file in attachement thank for your help AttachmentJehoster.zip (484 Downloads) |
8/19/2021 5:19 PM | |
Joined: 6/24/2010 Last visit: 5/25/2023 Posts: 8 Rating: (0) |
Yes , The actual master cave is 6ED-1052-1MD00-0BA8, and I would like to replace this one by a 0BA1 |
Follow us on