12/4/2015 6:26 AM | |
Joined: 2/21/2014 Last visit: 7/15/2024 Posts: 652 Rating:
|
Hi John I think you copied the code to left click of a button and try to run this script in Runtime. This is a VBA code and will not run in WinCC runtime. this is used to export the code to txt file offline from graphics designer. see attachment for more details of how to run this code. also the updated script is attached which will also close the files opened by running this VBA Macro. Try it and update the results or problems. I hope this works for you. All the best
Thanks, Harry AttachmentExportAllScripts.zip (576 Downloads) |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
This contribution was helpful to
3 thankful Users |
3/30/2018 8:55 AM | |
Joined: 2/21/2014 Last visit: 7/15/2024 Posts: 652 Rating:
|
Hi, Thanks for pointing out the missing things. i have modified it and uploaded it now. however OnOpen is not yet done. but i think you can get the idea from the scripts. welcome to point out other issues :) Thanks, HarrY AttachmentExportAlltheSCripts.txt (432 Downloads) |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
This contribution was helpful to
2 thankful Users |
11/20/2018 7:37 AM | |
Joined: 2/21/2014 Last visit: 7/15/2024 Posts: 652 Rating:
|
Hi, The attached script exports the direct link Tags, however, into a Text file. i hope you can export it to Excel or any other format and only the required fields. Import: I have not started work on import as not needed for me till now. but i hope to do it soon, don't know when. Thanks, HarrY AttachmentExport_Direct_Links.txt (400 Downloads) |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
This contribution was helpful to
6 thankful Users |
Follow us on