7/13/2008 10:39 AM | |
Posts: 86 Rating: (1) |
Hello! the Valve object doesn`t have a tooltip property.... is there any way to create a tooltip attached to it (only appears when the mouse hovers on it)?? |
7/13/2008 5:32 PM | |
Posts: 2661 Rating: (279) |
When you pick up an object from the symbols library, it will not have the tool tip property. Right click on the symbol to create a customized object as shown in theattachment. AttachmentDokument1.pdf (332 Downloads) |
Last edited by: Phantom75 at: 7/13/2008 5:36 PMcorrections |
|
7/13/2008 8:01 PM | |
Posts: 86 Rating: (1) |
Thanks Daniel, But i dont want to use a customized objects.... doesn`t vbs have any solution against this problem?? |
9/10/2008 6:05 PM | |
Posts: 2661 Rating: (279) |
Do you see the tooltip property in Object Properties, User Defined 2 in Graphics Designer? |
9/10/2008 6:24 PM | |
Posts: 14 Rating: (0) |
Yes I see it. I set also the text, but in runtime when I stay on it with the mouse nothing appear.
Attachmenttooltip image.zip (221 Downloads) |
9/11/2008 8:31 AM | |
Posts: 14 Rating: (0) |
yes the tooltip work for other WinCC objects! I have tried with a rectangle and it's ok!! Help me.... |
9/12/2008 2:34 AM | |
Posts: 2661 Rating: (279) |
Hi FabioIT, Can you post your PDL (with the customized object)? Thanks |
Follow us on