5/6/2013 10:04 AM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello Mehmet Emin, Please have a look at the following link: What connections are there between the version designations in WinCC flexible? When you have WinCC flexible 2004, you have the image: TP170A_micro_V7_0.img That is the one you need. Try to perform an OS update with the option "Reboot" how do you do an operating system update (OS update) on operator panels? Best regards, Wizard |
5/6/2013 11:21 AM | |
Posts: 25 Rating: (0) |
Hello Wizard, Thank you for your replay. I have installed OS on TP170micro. But I can not find TP170micro image. On Wincc Flex2004 to 2008sp2 there are just TP170A_micro image file. Aftre install TP170A image file I am trying to download application to TP170micro panel so can not connnect to panel. I try with USB/PPI cable and RS232.PPI cabel. I can install OS with both of that cables without any problem. But I can not download application to panel. I am using Wincc 2008 sp2. Switch settings on RS232/PPI cable is 11000000 for 115200baud. PPI led on cable is lighting always. But no action on RX/TX light. Please help. Thanks Attachmenttp170micro_pg_pc_settings.pdf (124 Downloads) |
5/6/2013 11:40 AM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello Mehmet Emin, Please have a look at the following link: how can you transfer a WinCC flexible project serially to a panel? Best regards, Wizard |
5/6/2013 2:02 PM | |
Posts: 25 Rating: (0) |
Dear Wizard Everything is ok like how explainied on support page. OS update is ok, but no download project. is there any others? |
5/6/2013 2:25 PM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello Mehmet Emin, When you want to download project to panel.The panel is in "Transfer mode"? Best regards, Wizard |
5/6/2013 2:36 PM | |
Posts: 25 Rating: (0) |
Hello Yes it is on Transfer Mode. Thank you |
5/6/2013 3:20 PM | |
Posts: 25 Rating: (0) |
Hello Wizard, Loader V07.02.03.00_01.55 When I set PG/PC interface to S7ONLINE ->PC/PPI then WinccFelx Download setting show like that. So how can I chose USB/PPI cable on WinccFlex Settings? Regards Attachmenttp170micro2.pdf (73 Downloads) |
5/6/2013 3:34 PM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello Mehmet Emin, Please have a look at this link: What transfer options are available in the various operator panels? The USB/PPI cable can not be used to transfer project (only for OS update) So you need RS232/PPI cable and a real COM port. Best regards, Wizard |
Follow us on