9/8/2010 6:26 PM | |
Joined: 6/20/2010 Last visit: 9/12/2025 Posts: 97 Rating:
|
Escribe texto o la dirección de un sitio web o traduce un documento. Escuchar Good afternoon, need help to structure a subroutine sync date and time, ie how they are used correctly and SET_RTC READ_RTC blocks between a CPU 224 and OP7 for it to synchronize with the CPU date and time whenever necessary. I use Protool respectively Microwin_32 and I have no clear what I'm doing wrong, because the CPU automatically changes my time as I say in Siemens. I do not understand any of the two manuals. Protool I have declared in the interface area pointer from the VW160 as an area of memory reserved for other operations such as changing the parameter screen 51. For date and time to transfer the parameter control 41 of Protool not know how to use it. Thanks and greetings to all. |
9/9/2010 8:12 AM | |
Posts: 2930 Rating:
|
Hi, have you checked the FAQ's how to synchronice the time in the S7-200 FAQ's. Goto www.siemens.com/s7-200 and select support FAQ's..... Then search for Time synchronization and you will find several FAQ's. I haven't seen one for your specific OP, but maybee the FAQ's help |
9/9/2010 9:38 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Dear Otobit, This link might help: how do you synchronize the date and time between a line or graphics device (TD17, OP5, OP7, OP15, OP17, TP27, OP27, TP37, OP37) and an S7-200 CPU with ProTool? Best regards, Wizard |
Follow us on