5/25/2016 8:06 AM | |
Joined: 9/21/2013 Last visit: 1/16/2024 Posts: 66 Rating: (1) |
Thanks bg2492, Please check the attached screenshot for TagLoggingFast settings do i have to increase days to 53 & as well as max size of single segment? How i can determine there are not segments more than 200? Thanks in advance Amol Attachmentsettings.pdf (250 Downloads) |
Last edited by: Amol V at: 5/25/2016 8:19:20 AMLast edited by: Min_Moderator at: 5/25/2016 11:37:17 AMConvert attachment to pdf |
|
5/26/2016 8:52 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Amol V, the number of 200 is a recommendation for a good performance, see: How many single segments can be connected to the SQL server in PCS 7 without impairing performance? https://support.industry.siemens.com/cs/ww/en/view/34473263 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on