12/4/2019 2:25 AM | |
Posts: 2 Rating:
|
Hi. I have a similar problem. I have a LOGO 8.FS4_1 connected through a switch to my PC. I try pinging the LOGO on 192.168.0.3 and I get no response. I can see that the logo is connected through soft comfort though. Any Ideas? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/04/2019 06:04:59New subject after splitting |
|
12/4/2019 4:17 AM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
Hello KidPLC, at first welcome to the forum. "LOGO! 8.FS4_1" is only the symbolic name of a FS4 LOGO! in a network project. Which LOGO! have you exactly? Please write the exact Siemens order number and the firmware version. Which IP address and subnet mask has the PC? Try to search the LOGO! in your network (see attach video) in a empty network project. If the sofware find the LOGO! in your Network, open the window with the properties of the LOGO!, make a screenshot and show us the screenshot. AttachmentSearching LOGO! in network project.wmv (178 Downloads) |
Follow us on