6/22/2024 11:58 AM | |
Joined: 6/22/2024 Last visit: 6/22/2024 Posts: 4 Rating:
|
I have the same problem. I'm using LOGO! Soft Comfort 8.4.0 and trying to connect to a brand new LOGO! This is my first time using Siemens PLC. I'm finding it very frustrating that won't just connect. Windows 10 PC using a USB Realktek ethernet adaptor. The ethernet adapter works fine for all other applications. I've tried two other USB ethernet adaptors and have the same result. I've tried the ethernet adaptor set to automatic IP and to fixed IP but unable to get it to connect. Note that when I click the blue refresh arrows it comes up with the correct MAC address shown on the screenshot show the correct IP, Subnet mask, gateway and MAC address of the LOGO! device. So it is reading this data from the device. Also note along the top "Connect ~though: Ethernet ....." the next box is blank. There is nothing in the drop down menu. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/24/2024 04:46:36New subject after splitting |
|
6/22/2024 1:09 PM | |
Joined: 12/18/2014 Last visit: 6/29/2024 Posts: 33262 Rating:
|
Which IP address has the USB adapter? |
6/22/2024 2:06 PM | |
Joined: 12/18/2014 Last visit: 6/29/2024 Posts: 33262 Rating:
|
Then LSC does not recognize your USB adapter. Why? I don't know. |
6/22/2024 3:37 PM | |
Joined: 6/22/2024 Last visit: 6/22/2024 Posts: 4 Rating:
|
Is there an update to LSC that I could update to? I'm using v8.4.0 |
Follow us on