8/6/2016 10:17 PM | |
Posts: 2 Rating:
|
hi can you help with my problem. I am trying to connect to the Siemen logo 0BA8 12/24 RCE. I have written a program for the first time. I have bought the software for the 0BA8 and it came with a green Ethernet cable. I have plug the green cable into my laptop and also in the 0BA8 and tried to connect the unit to transfer my program into the unit, but I get an information box come up. I will write the information below what it is asking from. here goes. IP Address of your PC and the target LOGO are not in the same subnet. the application try to add an additional local IP Address, do you want to continue". I do not know how to proceed in order to communicate with LOGO in order to up load my program. can you help with my problem please. I would grateful if you could put me in the right direction. thank you Mr D Gore ------------------------------------------------------------------------------------------ Closed cause question published twice. Please discus here: ethernet issues |
Last edited by: CS Moderator at: 8/8/2016 12:35:52 AMNew subject after splitting |
|
Follow us on