1/14/2015 10:55 AM | |
Joined: 12/18/2014 Last visit: 7/11/2024 Posts: 33328 Rating:
|
On this page of Siemens there are examples of communication 0BA7 <> 0BA7. Either master / master or master / slave. I would prefer the master / master link. In master / master in each logo is a standalone program, for master / slave is only one program in the master logo, the slave logo is then only as an extension module. http://w3.siemens.com/mcms/programmable-logic-controller/en/logic-module-logo/application-examples/Pages/Default.aspx |
This contribution was helpful to
1 thankful Users |
1/14/2015 11:55 AM | |
Joined: 12/18/2014 Last visit: 7/11/2024 Posts: 33328 Rating:
|
I'm sorry, I don't know that. |
1/14/2015 12:19 PM | |
Posts: 13 Rating:
|
ok, I've checked it, in master/slave communication delay is similar. |
Follow us on