2/27/2006 9:47 AM | |
Joined: 12/5/2005 Last visit: 8/9/2021 Posts: 289 Rating:
|
I've gone through the screen I posted, replacing almost all of the script with the dynamic dialog connections. The update for that screen is less than two seconds, compared to the original 2 minutes. It's been a head-scratching day or two, but the result is worth it. I'm posting the new version so anyone who still has the last one can compare. Thanks for the help [:D] AttachmentMix-Tank2.zip (549 Downloads) |
3/9/2006 8:59 AM | |
Joined: 1/17/2006 Last visit: 5/20/2025 Posts: 800 Rating:
|
You can share the picture with us. Maybe we can help. |
3/10/2006 12:41 PM | |
Joined: 12/5/2005 Last visit: 8/9/2021 Posts: 289 Rating:
|
OK. Quick explanation - the Recipe screen has provision for up to 40 Recipes Each Recipe can have up to 16 steps, each with 13 variables (most are operator-inputs). When the screen is first shown, whenever the Re-Load button is pressed, or whenever a Recipe is selected (by clicking on the Recipe Name field just above the table), a script calculates the name of the tags required, and loads the values. AttachmentRecipe1.zip (563 Downloads) |
Follow us on