11/5/2019 7:03 AM | |
Joined: 4/6/2019 Last visit: 2/17/2024 Posts: 53 Rating:
|
HI I have a question for update firmware ? I decide change a pxc version v5 to desigo v6 ? I rode a xwork help ? Who has a cable diagram ? for RS232 Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/05/2019 08:11:46New subject after splitting |
|
11/5/2019 11:43 AM | |
Joined: 7/25/2012 Last visit: 6/12/2024 Posts: 259 Rating:
|
Hello, there should be used the pins from plug (G) RJ45: 3-GND, 7-TxD, 8-RxD, you can see on the datasheet CM1N9222en_15.pdf - link https://www.downloads.siemens.com/download-center/Download.aspx?pos=download&fct=getasset&id1=A6V11272745 The connection diagram with the adapter from RS232 to RJ45 is attached. |
Best regards, |
|
11/5/2019 6:44 PM | |
Joined: 11/8/2017 Last visit: 6/26/2024 Posts: 328 Rating:
|
Hi, Not sure if you seen my post here? (The thread was getting a bit mixed up between Desigo and Apogee controllers). To do this, you'll need a USB to 232 (FTDI type) adaptor, a PXA-C2 adaptor from Siemens, and a standard ethernet patch lead to connect to the controller HMI port. If your PC/laptop has an old serial / RS232 port - then you can exclude the USB to 232 adaptor. The PXA-C2 doesn't cost much, and make things that little bit easier. Regards, |
11/6/2019 9:42 AM | |
Joined: 4/6/2019 Last visit: 2/17/2024 Posts: 53 Rating:
|
Hello, thank you? Do you update the firmware with RS232? I updated pxc with pc adapter !! to be sure in this way we do not need a pc adapter ?! best regards |
11/6/2019 9:46 AM | |
Joined: 4/6/2019 Last visit: 2/17/2024 Posts: 53 Rating:
|
dear cj Hello, thank you? Do you update the firmware with RS232? I updated pxc with pc adapter usb to pxm10 port !! to be sure in this way we do not need a pc adapter ?! best regards
|
Follow us on