4/24/2010 4:26 AM | |
Posts: 90 Rating: (0) |
Dear Users, |
4/26/2010 6:02 AM | |
Joined: 5/12/2006 Last visit: 10/18/2024 Posts: 22422 Rating: (3023)
|
Hello, what is displayed on the BCD Display of the D435? Regards Christoph |
4/26/2010 8:14 AM | |
Posts: 116 Rating: (7) |
Hi, which CF card you are using? Might be not the correct boot loader. see compatibility list (chapter 2.5): http://support.automation.siemens.com/WW/view/en/18857317 Regards Jerry |
4/27/2010 6:32 AM | |
Posts: 90 Rating: (0) |
Hello, I´m using a 64Mb CF card. Sorry my mistake, but I´m using SCOUT V4,1 SP4 (instead V4.1 SP2 as I have mentioned before). In the Scout DVD there are two Firmware folders from V4.1.4.1 : 1) V4.1.4.1 > PN_V2.1_and_DP > D4XXX_SINAMICS_V2.5 > all firmware files 2) V4.1.4.1 > PN_V2.2 > D4XXX_SINAMICS_V2.5 > all firmware files So, which one should I use (from PN_V2.1_and_DP or PN_V2.2 folder) ? How to know ? And is the bootloader file included to write boot sector ? Just to remember my first post "How can I activate the Software Limit Switch using <Axis>.swlimit.state system var in a LAD program ?" Thanks in advance. Greetings, Denker |
Last edited by: Denker at: 4/27/2010 6:34 AM |
|
4/27/2010 9:45 AM | |
Joined: 5/12/2006 Last visit: 10/18/2024 Posts: 22422 Rating: (3023)
|
Hello, <Axis>.swlimit.state:=ACTIVE Regards Christoph |
This contribution was helpful to1 thankful Users |
Follow us on