6/27/2022 7:50 AM | |
Joined: 9/3/2008 Last visit: 9/19/2024 Posts: 928 Rating: (162) |
Hi If you buy a license (new or upgrade) as a download, you obviously need a computer with internet access. But it does not have to be the computer with the Step7 software installed. It can be any computer that pnly has the License Manager software installed. This can be downloaded from License Manager Download page. After you install this on any computer that can connect to the internet, you can download the license and transfer the license to a usb for example. If possible, you could connect the computer to the same network as the Step7 computer and transfer the license directly by network. If you transfer the license to a usb, you just need to connect the usb to the target device and transfer the license onto the target device with the License Manager already installed here. Best regards |
Michael |
|
This contribution was helpful to1 thankful Users |
Follow us on