2/18/2012 2:32 AM | |
Joined: 3/28/2007 Last visit: 1/3/2024 Posts: 40 Rating: (0) |
Dear Prakash, I find the attached document in the 802D SL tool box. The problem is that there is no explanation given how to switch between the second and third encoder. I understand from the document that the dual track encoder cannot be used as it says that the First (motor encoder) and the Third Encoder should have the same resolution. It means that the third encoder should have 2048 PPR as that of the motor encoder.The second encoder can have a different resolution and hence 9000 PPR encoder can be used. It would be very helpful if you could read the attached file and advice me how to switch between the second and third encoder. Thanks in advance Chandhaa AttachmentCommissioning of third sensor.pdf (79 Downloads) |
Follow us on