8/5/2015 12:45 PM | |
Joined: 9/3/2010 Last visit: 5/23/2024 Posts: 17 Rating: (3) |
I need to create navigation buttons on WinCC picture window. I manage to make use of the demo project navigation VBS script to perform the job on direct picture window (Main_Display). However, the structure of the navigation is laid out in such a way that it has picture window within picture window (refer to attach), and suppose to work only with button. Thus that may be more straight forward. Right now, I will have to add another button at the base screen, to activate the screen change on the picture window (Process_Picture) within a picture window (Main_Display). I tried various method but got error on the script during runtime. Wonder can you help with this? I tried to change the following from the code, but it does not work... Set objGraphicView = HMIRuntime.Screens("Main_Display").ScreenItems("Process_Picture") - working example from demo project - Public Function Navigate(NavigationModus) Dim objGraphicView,i,strStartBildName For i = LBound(arrPictures) To UBound(arrPictures) AttachmentNaviStruc.pdf (171 Downloads) |
8/5/2015 2:51 PM | |
Joined: 9/3/2010 Last visit: 5/23/2024 Posts: 17 Rating: (3) |
Hello Georg, Appreciate your quick reply! I will study and try again. Will feedback should it work, or not work. Thanks. |
Follow us on