5/6/2016 2:28 PM | |
Joined: 8/15/2015 Last visit: 6/24/2024 Posts: 130 Rating:
|
Dear Isoto this is a more manual or mathematical way to do it ... but it can work sure , Because I am really new to this, I just try to get all the aspects of the software in order so that I can do a nice software to run nicely, and be remotely operated and controlled and all of the above Thank you In advance Le Test !!
|
5/6/2016 3:13 PM | ||
Joined: 12/16/2012 Last visit: 7/11/2024 Posts: 652 Rating:
|
Hi! As I know, Step 7 Basic contains also the simulator. You can start TIA and click on the HELP tab / Installed software .... and then in the lower part of the pop-up click on "Detailed information about installed software" to see what you have. |
|
This contribution was helpful to
1 thankful Users |
5/7/2016 6:00 AM | |
Posts: 58 Rating:
|
Hi Le Test What is your definition of Weekly timer I understand the next concept A) You need to start a motor or oven all the monday at 5:00 AM , B) You need to Stop a motor or oven all friday at 11:00 PM C) You need to start or stop device depende of the weekday and the time If this is your concept of Weekly timer my sugestion work good But if your concept of Weekly timmer áre the next : A) You Define a time for example 2 day 8hrs and 23 min and you need to measure this time Do you need to make your timer with two IEC timer and one counter |
This contribution was helpful to
1 thankful Users |
11/11/2016 1:58 PM | |
Joined: 8/15/2015 Last visit: 6/24/2024 Posts: 130 Rating:
|
Dear Isoto , I found a DLL library that had this integrated in one block the weekly timers and yearly timers and e.t.c https://support.industry.siemens.com/cs/attachments/78788733/78788733_s7-1200_dtl_timer_v10_en.pdf here is the PDF , manual , is coded with the old V12 but still I managed to upgrade it , no i need to test it :D if this works out of the box I am in business :D Thank you in advance Le Test !! |
Last edited by: Min_Moderator at: 11/14/2016 1:16:18 PMReplace link |
|
11/11/2016 11:35 PM | |
Joined: 6/24/2013 Last visit: 7/5/2024 Posts: 1609 Rating:
|
Hi if You need: 1. a weekly interval (i.e. 7 days apart; regardless of hour): you can use IEC Timer (it covers up to 21ish days) 2. if you want to trigger an event on a specified hour (i.e. monday, 0600hrs): - read system time and when it is more equal setpoint: 1. check monday before or at last execution date. 2. after execution remember the date in a data block this way you do thing once a week or on first opportunity in given week (i.e. when PLC is OFF at time of scheduled time) I did this for data logging in Citect SCADA. Script is below (should be easy to convert to SCL in S7-1200/1500): // Function checks if files needs to be moved to C:\OLD_LOGS and makes this happen when needed. |
This contribution was helpful to
1 thankful Users |
11/11/2016 11:58 PM | |
Joined: 8/15/2015 Last visit: 6/24/2024 Posts: 130 Rating:
|
Dear all , Things got very complicated very fast :'( , Why these people don't just have something similar like in logo 8 , A Weekly timer and that's it ? oufff .. I will try to figure it out , Thank you all for the feedback I really appreciate it :D Thank you in advance Le Test !! |
Follow us on