5/9/2008 8:10 PM | |
Posts: 2661 Rating: (279) |
Yes interrupt OB will be OB40 with priority 16 (highest).
If you trigger the OB40 processing with multiple interrupt inputs, you can determine which input triggered the interrupt by simply scanning the inputs. For example: A I 10.0 logic A A I 10.1 logic B The inputs (process images I 10.0 & I 10.1)will be updated before the interrupt is triggered. Regards AttachmentDokument1.pdf (694 Downloads) |
This contribution was helpful to1 thankful Users |
5/10/2008 10:17 AM | |
Posts: 80 Rating: (2) |
I think, yes ! Thanks Phantom75! pici_c |
Follow us on