3/27/2019 8:01 AM | |
Joined: 4/4/2018 Last visit: 8/26/2024 Posts: 101 Rating: (1) |
Hello We are using TIA portal V14 sp1 and CPU 1517 F. In Graph if the interlock is not healthy and Transition is healthy then it jumps to the next step with out any error.What we want is the PLC should trigger an error if the interlock is healthy no matter what the transition condition is.The machine should stop and run only if the operator acknowledges the alarm. How or Where we can specify that the operator must acknowledge an interlock alarm. Thanks in Advance Anoop Balagopal ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/27/2019 11:04:34 AMNew subject after splitting Last edited by: anoopbalagopal at: 3/27/2019 11:10:34 AM |
|
3/28/2019 7:10 AM | |
Joined: 5/6/2010 Last visit: 9/2/2024 Posts: 1978 Rating: (275) |
Hello Anoop, please have a look to the functions of ProDiag. Please look at this link: Machine and Plant Diagnostics with ProDiag Prodiag is possible with a firmware >2.0. |
Last edited by: Jen_Moderator at: 3/28/2019 2:04:52 PMOptimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on