2/13/2024 10:00 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16438 Rating:
|
Hello If you want to run only a WinCC Professional RT on the IPC then you only have to insert a PC Station in your TIA Project then insert a WinCC RT Professional and a IE general Networkcard. Then you can set up everything including the PLc connection in the TIA Project. On the IPc you only have to install WinCC RT Prof and Simatic Net PC Software. Set PGPC Interface and thats it.... To download the project just load the WinC Prof RT to the IPC, you do not have to dowload the PC Station HW or go online to the PC Station! LINK Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on