1/15/2013 9:07 AM | |
Joined: 10/3/2010 Last visit: 6/14/2024 Posts: 1552 Rating:
|
Someone has more knowledge and experience about communication possibilities between WinCC (OPC?) and Mitsubishi A3A CPU (AJ71C24-S8) and also Q03UDE CPU (QJ61BT11N)? thanks in advance. |
B r g d s , |
|
1/16/2013 2:39 PM | |
Posts: 1530 Rating:
|
Hello SteBo, I think you need detailed help of real OPC experts. Maybeit would be a good thing toconctretize your problem a little bit? For all OPC beginners, who will find this thread I give some general information: You have to find out which way yourcontroller can be connected via OPC to WinCC. Therefore you have to ask producer or look into documentation of controller. For sure WinCC can communicate via OPC. More information is available in the WinCC Information System in this path: WinCC Information System > Tools > OPC - Open Connectivity Best regards Bizur |
1/17/2013 2:36 PM | |
Joined: 10/3/2010 Last visit: 6/14/2024 Posts: 1552 Rating:
|
thanks both of you for replying @GoForIT, do you know more specific about Kepware OPC and Mitsubishi A3A CPU with AJ71C24-S8 card cause Kepware itself doesn't really know if their OPc will work with A3A CPU. The port on A3A is occupied. On the AJ71C24-S8, rs232 port is used, rs422 port is free. cheers |
B r g d s , |
|
1/18/2013 9:50 AM | |
Joined: 10/3/2010 Last visit: 6/14/2024 Posts: 1552 Rating:
|
not at this point cause it's not yet an actual project. Meanwhile, I've been informed to install an AnS series ethernet card in the old A3 PLC. |
B r g d s , |
|
1/21/2013 10:13 AM | |
Posts: 1530 Rating:
|
Hello SteBo, I suppose this thread can be closed now, because of GoForITs assistance. If this should not be done just post it. Best regards Bizur |
Follow us on