12/20/2011 3:31 PM | |
Posts: 154 Rating:
|
Hello, at first you have to configure you start and stop time in LOGO! Soft Comfort in the VM Mapping. At next you have to configure a connection in WIN CC Flexible, you have to use S7-200 at communication driver. In the next step you have to configure your variables, there you have to use the some addresses like in LOGO! Soft Comfort.I have attached you a screenshot, but I only have TIA V11, but I think in Win CC Flexible it is the same.Also have a look at the following link: How can you set up a connection between a LOGO! 0BA7 and an HMI Panel? I hope this help you. Best regards |
10/17/2012 12:51 PM | |
Posts: 8 Rating:
|
hello i have the some probleme. Did you manage to fix it? Victor Bors QM |
Follow us on