3/1/2013 11:18 AM | |
Posts: 3037 Rating: (192)
|
Hello, You can use PRODAVE for communication with PLC and an Application. SIMATIC PRODAVE MPI/IE V6.0 Tweety |
3/6/2013 9:25 AM | |
Joined: 9/2/2012 Last visit: 6/3/2019 Posts: 176 Rating: (16) |
As i understand fromthis pagei need a license for ProDave to work, correct? If so, is there some other way i can make this work with an WinCC RT without the need for yet another license? Or do i have to result into text-files to pass data/strings along between my C# and HMI?
|
3/8/2013 11:07 AM | |
Joined: 6/20/2011 Last visit: 5/21/2024 Posts: 74 Rating: (7) |
U can use Txt files from the VB script editor in wincc or try Libnodave... its a free DLL to exchange data |
Follow us on