7/14/2015 10:56 AM | |
Posts: 11 Rating:
|
wincc flexible 2008 sp3 installation problem with windows 7 professional sp1 HI friend i using OS is windows 7 professional sp1 and i was installed tia portal v13 and it is working fine now i tried to install wincc flexible 2008 sp3 in the same OS but it couldnt installed there and it showing some error but in the installation guide mention it will support with windows 7 professional sp1. and i attached what was shown while installation. please help to me
---------------------------------------------------------------------------------------------------- |
Last edited by: jhon benil at: 7/14/2015 10:58:06 AMLast edited by: Min_Moderator at: 7/14/2015 2:12:01 PMNew subject after splitting |
|
Follow us on