7/16/2012 4:57 PM | |
Posts: 3037 Rating: (192)
|
Hello newyguy, You should do the point 2.1 in the following FAQ. What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted? Tweety |
7/16/2012 6:20 PM | |
Posts: 4 Rating: (0) |
thanks for the tip but I've already read through all that page and did all the points necessary including 2.1 but still no luck. I'll keep trying to fix it and I appreciate it if anyone else have other solutions to share. I think the last option would be to re-install the whole windows 7. |
7/17/2012 3:26 PM | |
Posts: 3037 Rating: (192)
|
Hello, You shouldcheck the list on the end of the following FAQ: With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible? Do you do a repair instalation of WinCC flexible? Tweety |
7/18/2012 4:59 PM | |
Posts: 4 Rating: (0) |
my wincc flexible is 2008 sp3 which is compatible with 7 x64 I installed it once. then completely removed it with all the SQL programs I had (all of them) from add and remove. then installed wincc again. should I repair it? |
Last edited by: newyguy at: 7/18/2012 5:00 PM |
|
7/19/2012 11:02 AM | |
Posts: 3037 Rating: (192)
|
Hello Yes, you should use the repair installation of WinCC flexible. Tweety |
9/17/2013 7:49 AM | |
Posts: 53 Rating: (2) |
Hello, I still have the same problem ... I´ve tried everything. I did every point fromhttps://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=29420408&caller=view, i even returned to clean system and tried to install it on it, but still the same (installed without problem but then apears info about cannot create template, or cannot connect to the configured SQL ...). If anyone know any solution, or can give me any idea pls help. Henio.
|
9/25/2014 5:35 AM | |
Joined: 3/2/2012 Last visit: 5/21/2024 Posts: 45 Rating: (0) |
Thanks all, specially Tweety I face the same problem and it solved |
9/26/2014 11:04 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published byHD86is split to a separate thread with the subject simatic flat panel project creation problem. Best regards Min_Moderator |
Follow us on