6/2/2014 5:12 PM | |
Joined: 4/19/2008 Last visit: 6/6/2024 Posts: 1525 Rating: (159) |
Hello koayyk, Is already project is running on the MP ? if not then you can do the reset to Factory setting. How can you reset WinCC flexible to the original status of the last installation? How do you do an operating system update (OS update) on operator panels? In this Look for "Operating system update" or "Reset to factory settings" with WinCC flexible Have a Look on the FAQ for the WinCC Transfer setting How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? |
Ammy |
|
This contribution was helpful to1 thankful Users |
6/2/2014 6:39 PM | |
Posts: 784 Rating: (52) |
No FollowAmmy advise. |
This contribution was helpful to1 thankful Users |
Follow us on