6/20/2014 7:16 PM | |
Posts: 2661 Rating: (279)
|
Check the WinCC Premuim Addon Shutdown WinCC: http://w3.siemens.com/mcms/human-machine-interface/en/visualization-software/scada/wincc-addons/Pages/Default.aspx |
6/22/2014 1:37 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello justino This is a common problem with WinCC. We have experienced frequently the WinCC Project ( Sometimes the complete WinCC Installation ) crashes if PC is switched off without shutdown. The problem is generally not faced in HMI / SCADA softwares ( Or al least the chances of the problem occuring are much lesser ) where a "Compiled" project is used in Runtime. ( e.g. Protool-Proor many Third party HMI Packages ). However sometimes even the Windows itself can get corrupted in such cases where PC is switched off without Shutdown. The only solution is to keep a backup copy of the project which can be immediately used in case of the running project getting corrupted. However the Runtime Data / Archives would be lost in such cases. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on