9/16/2016 4:16 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello JSLOJSLO If you use a Server Client system then only the Server has a Communication to the PLC. In this case the Systems must have a connection to each other. But if the server is down or the Client looses Connectoin to Server then you cannot use any of the two OS. With Webnavigator its quite the same the only difference is that the Webclient is a much simpler Softare than the Client installation and you could also use an office PC. If you want to use two Single User Stations OS so every of these yould work without needing the other then look at this FAQ for Communication requirements: https://support.industry.siemens.com/cs/ww/en/view/98699910 But I Think you should contact you Siemens Sales or Presales Contact. They could help you to create a proper solution. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on