10/10/2016 9:52 AM | |
Posts: 7 Rating:
|
Hi everyone, I have same problem that I had already installed WinCC RT professional update 9. What I want is start runtime on PC(installed WinCC RT professional) with real PLC. But the button "Start runtime on PLC" still not active. Then I try to make .mcx file by go "Online" >Download to file system. After that I run WinCC RT start and select the file and run it. But it still don't work when I hit the button "start" and "stop" (My PLC is already in Run mode). And PC IP is the same with PC_system1. Please see the attach files. Can someone tell me Procedures to start runtime on PC with real PLC? plz help. Thanks! ------------------------------------------------------------------------------------------ Attachmentimages.zip (368 Downloads) |
Last edited by: Min_Moderator at: 10/10/2016 11:51:30 AMNew subject after splitting |
|
10/10/2016 10:30 AM | |
Posts: 7 Rating:
|
Hi ChristophD , Thank you very much! You made my day :)) Tien |
10/11/2016 5:00 AM | |
Joined: 9/30/2016 Last visit: 2/11/2025 Posts: 7 Rating:
|
Bạn khắc phục như thế nào v? |
10/20/2016 8:35 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Dear QThangdotnet, this is a English forum. Can you write your question in English? With best regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
12/17/2016 4:47 PM | |
Posts: 7 Rating:
|
Hello, You can do it by following steps: S1. In your HMI tree > Connections> At the "Access point" choose "S7 ONLINE". But make sure you already have HMI connection. Please see the picture I attached below ( Chỗ Access point chọn S7 ONLINE nhé, xem ảnh để rõ hơn) S2. Control panel > you search " Set PG/PC interface" > In the "Access point Application" select "S7 ONLINE --> Driver (Realtek PCIe...) Hope this helps, Brs, Tien Attachmentconfig.zip (443 Downloads) |
Follow us on