5/24/2011 8:15 AM | |
Posts: 799 Rating: (43)
|
Hi Jaapie,
I think this generally should work, because in WinCC Information System is following information: click here I guess, that the problem is something else, but actually don't know where best regards |
5/24/2011 9:39 AM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Also with this description, I do not think FPT'swill work. It does not describe FPT.Or do I have to look closer? |
5/24/2011 10:12 AM | |
Posts: 799 Rating: (43)
|
Mhh...Maybe you are write! I don' thought about the difference between FP and FPT. regards |
5/24/2011 3:26 PM | |
Joined: 10/3/2010 Last visit: 10/17/2024 Posts: 1562 Rating: (192) |
there ain't much clear info on this but if you check the DemoProjectV7 or PraxisDemoV7 http://support.automation.siemens.com/WW/view/en/35102867 both seem to have faceplates in the WebNavigator\Pictures folder maybe worth to try one of these demo's? |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
5/25/2011 8:47 AM | |
Joined: 10/3/2010 Last visit: 10/17/2024 Posts: 1562 Rating: (192) |
Now it gets confusing, in WinCC v7 standalone (not intergrated in S7), normal pictures have the extension .pdl , faceplates have an extension .fpt |
B r g d s , |
|
Follow us on