3/17/2020 10:38 PM | |
Joined: 11/17/2015 Last visit: 5/3/2024 Posts: 57 Rating: (16) |
Hello. I have several remote stations with configured WebUX interface (WinCC 7.4). Few weeks ago in some browsers (for example Google Chrome 80.0...) I began to receive warnings, that connection is not fully secure, but I have valid certificates installed on machines with WebUX. I found an article where is described that SSL 3.0 / TLS 1.0 is now deprecated and soon all browsers will start to show full screen warnings I've try to configure Windows 7 IIS to work with TLS 1.2 as described here, but no result So, basically, my question is: does WebUX support TLS1.2? If it does, what should I do to make it work? Change operating system to Windows 10 or get some kind of new certificates or... install old version browser? |
3/31/2020 3:19 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hi, i think you just need to create a new certificate? B.R. |
Grundkurs/Systemkurs WinCC V7: |
|
4/13/2020 10:30 PM | |
Joined: 11/17/2015 Last visit: 5/3/2024 Posts: 57 Rating: (16) |
Hi. Thank you for your answer. For example, same 2048-bit RSA certificate should work with SSL3.0 and with TLS1.2 also. So question is open Have anybody tried to make WebUX work through TLS1.2? |
Last edited by: xsmart at: 04/13/2020 22:46:05 |
|
Follow us on