10/16/2016 7:07 AM | |
Joined: 6/5/2014 Last visit: 4/25/2021 Posts: 109 Rating: (1) |
Any update Please ? |
10/17/2016 9:13 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Dear Mahmoud.Hazem, Please provide us more information : What do we need to solve your problem?1) Which kind of panel you're using ? 2) Do you have another PLC that you're using or is this fanuc the only 'plc' you're using ? If you have a siemens plc , you could look for the opportunity to add this Fanuc plc in the hardware configuration of your siemens PLC, by doing this you can communicate with wincc flexible through your siemens PLC... 3) Please give us more details how you want this panel to operate... Regards, Omega |
Last edited by: OmegaProjects at: 10/17/2016 9:27:02 AM |
|
This contribution was helpful to1 thankful Users |
10/17/2016 9:33 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
You can already check these FAQ's , but please provide more information about the purpose and configuration :) Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?What connecting cables are there for connections between the operator panels and the different controllers?Regards, Omega |
This contribution was helpful to1 thankful Users |
10/17/2016 1:14 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Hi Mahmoud.Hazem, Please follow manual (in link) chapter 3 : Communication with GE Fanuc controllers Regards, |
This contribution was helpful to1 thankful Users |
10/20/2016 7:11 PM | |
Joined: 6/5/2014 Last visit: 4/25/2021 Posts: 109 Rating: (1) |
Please Help as it's an important issue |
Follow us on