8/25/2010 10:24 AM | |
Joined: 1/4/2010 Last visit: 6/7/2024 Posts: 650 Rating: (40)
|
Hi Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x: http://support.automation.siemens.com/WW/view/en/6944907 |
Last edited by: Romulus at: 8/25/2010 10:24 AMRegards |
|
8/30/2010 10:12 AM | |
Joined: 8/21/2008 Last visit: 6/6/2024 Posts: 7 Rating: (2) |
Make a shortcut to WinCCViewerRT.exe Right click on the shortcut-> Properties -> Shortcut Tab -> Target: Add the location of the XML file between double quotes. You can change the XML file with for examplenotepad.The only thingI don'tknow is howto add a password because it is scrambled in the XML file... AttachmentWinCCViewerRT.zip (1314 Downloads) |
8/30/2010 11:58 AM | |
Posts: 12 Rating: (0) |
Thanksa lot. That helped. |
12/30/2010 9:48 AM | |
Posts: 1 Rating: (1) |
You can also use the hotkey "Ctrl + Alt + P" when WinCCViewerRT is running to open property window. |
This contribution was helpful to3 thankful Users |
7/14/2011 4:39 AM | |
Posts: 3 Rating: (0) |
Or go to the CMD prompt and enter 'winccviewerrt ?' to get the popscreen. |
This contribution was helpful to1 thankful Users |
8/29/2014 4:47 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
new question published by zara-90is split to a seperate thread with the subjectwhere can i get WinCCViewerRT.exe. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on