8/18/2009 9:10 AM | |
Joined: 1/27/2009 Last visit: 9/17/2024 Posts: 172 Rating: (8) |
Dear experts, I am in need to start to use STEP 5 as my company decided to obtain an old line which is under control of S5 series controllers. When i start Step5 -the fixed width and height window opens, so when i go online i do not see a full comment, only a part, because window width is to small. Is it possible to expand the width and height of STEP5 window? I have tried Window size of STEP5 V7.1 under WinNTbut result wasn't that i expected. I am using WinXP Pro SP2 and STEP 5/ST V7.23 Basic package. Regards Arturas |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
2/27/2010 2:57 PM | |
Posts: 3 Rating: (0) |
Kindly, press ALT key with ENTER key after opening s5 window. this will maximize your s5 window. |
This contribution was helpful to1 thankful Users |
Follow us on