5/16/2012 4:11 PM | |
Posts: 14 Rating:
|
I have aconnection betweena6.2 andwinccs7-300 withanOPC Server.how to connectdirectly withoutopc? thank fron santiago de chile
|
5/16/2012 4:55 PM | |
Posts: 14 Rating:
|
thank you , Ammy |
5/17/2012 10:19 PM | |
Posts: 14 Rating:
|
does not work withoutOPC, throughtcp/ ip, I need toconnect awireless signalvariable, I need helpplease, thanks. add example in PDF format
Attachmentsin opc.pdf (165 Downloads) |
5/17/2012 10:52 PM | |
Posts: 14 Rating:
|
-ip CPU is 192.168.0.3 - accepting ping in ip -yes,are you using Step 7 on the Same laptop is communication with S7-300 & Step7 working -im using opc kepware, i need work without OPC. thanks Attachmentping.pdf (133 Downloads) |
5/18/2012 3:04 PM | |
Posts: 14 Rating:
|
Can you Stop the OPC Kepware & then try, What it is Result.....? |
5/18/2012 3:04 PM | |
Posts: 14 Rating:
|
can not stop, I may have to uninstall |
5/18/2012 5:40 PM | |
Posts: 947 Rating:
|
Hello clinja You can write an application to share with WinCC, and to organize exchanges between the application and WinCC. Using the means of c, ODK, you can directly access a specific DLL, and solve the problem. But I would like to know - for what purpose you need to do what others have done? if you want to write my Scada, it is reasonable to use the OPC and create an environment for him. It will be a more universal. |
Follow us on