9/25/2020 7:45 PM | |
Joined: 2/10/2006 Last visit: 3/21/2024 Posts: 147 Rating:
|
Hello, There is no tool that allows conversion of APT programs to S7. You would need to rewrite the application. if you are using a lot of SFC in APT and you also need a visualisation system, you may want to consider using a PCS7 light version, which would allow to develop a software solution that is closer to the original APT code. Alternatively you could consider using the New Janus CPU from CTI which is also programmed in an IEC 61131 programming environment. http://www.controltechnology.com/products/2500-Series-Classic/processors/2500P-J750 Here some parts of the APT code could be imported but still some manual work would need to be done. If you want more information about this send me a private message. Regards, Carlo |
This contribution was helpful to
2 thankful Users |
Follow us on