6/24/2014 11:48 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! I dont not if it feets your needs, but why not to use breakpoints in that case? Please lookthis postand then ask additional questions. Hope it helps.
|
6/24/2014 3:41 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Not sure I understood you correct, but take a lookhere. Is that what you mean? |
6/26/2014 4:00 AM | |
Joined: 10/7/2005 Last visit: 5/7/2024 Posts: 3004 Rating: (1046) |
Hello sbjones8 S7 Professional does unfortunately not have any trending capability. While you can of course use WinCC for this, allow me to suggest you have a look at ibaPDA-S7-Analyzer. It is the "tool of the trade" as far as I'm concerned for all S7 related commissioning, troubleshooting and process optimisation purposes. Once you start using it, you'll wonder how you ever didyour S7 work without it and attached is also a case study for your perusal (also available from the Applications section of the iba webpage). Having saidall that, the disclaimer with this advise is thatI do also work for iba Oceania(I'd give youthe same advise thoughif this wansn't the case, and yes, there are also other third party S7 data logging tools out there). AttachmentApp_S7_Troubleshooting_OreProcessingPlant_EN.pdf (123 Downloads) |
Cheers |
|
This contribution was helpful to3 thankful Users |
6/28/2014 11:07 AM | |
Posts: 8946 Rating: (999) |
Have a look here as well: http://www.r-u-w.de/EN/Products/plc_scope.php |
This contribution was helpful to1 thankful Users |
Follow us on