7/15/2023 2:06 PM | |
Joined: 8/3/2022 Last visit: 7/19/2023 Posts: 1 Rating: (0) |
Has anyone run into an issue where the actual current of the G120X is different than what is being read by the S7-400 PLC? I have changed the p2000...2006 parameters inside the G120 to match the motor nameplate. I have also changed the PZD scale highs to match the VFD parameters. The drive is reading ~12A, but the PV_Drive block is outputting ~50A. On a side note, the yellow wrench beside all four PZDs from the VFD in the PCS7 faceplate indicates an issue with? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/17/2023 09:23:57New subject after splitting |
|
Follow us on