1/25/2024 12:18 PM | |
Joined: 1/25/2024 Last visit: 2/19/2024 Posts: 2 Rating:
|
I have a C# applicaiton using the Openness API managed to create a PLC (CPU 1518F-4) and a ET200SP. I have also managed to connect the PLC with the ET200SP with a subnet to the ProfiNet connections on both devices with the Openness API. When I check the connection in the TIA Portal/Step7's Device & network view, I still see the "Not assigned" label on the ET200SP. This should have the same name as my PLC.
How do I change the label on the ET200SP? When I connect the ET200SP to the PLC in Step7 I get the result I want. Please see the image below where the label on the ET200SP says "VccMachine". With my C# program I still have the "Not assigned" label instead of "VccMachine. Please see image below. I know this is possible, because this video at time index 32:17 shows how a lot of ET200SP devices get connected and the label is set to the name of the PLC. Please help! Openness V19 |
Last edited by: Jen_Moderator at: 01/26/2024 07:20:45Video embedded. |
|
Follow us on