6/20/2023 11:21 AM | |
Joined: 9/2/2021 Last visit: 7/22/2023 Posts: 3 Rating: (0) |
Hi, I am facing a hardware communication issue between S7-1215 and PAC 3200 with the Profibus expansion module (7kM9300-0AB0-0AA0). In the TIA portal, only the Profibus expansion module (7KM9300-0AB01-0AA0) is available which does not match with the hardware. I install the GSD file for the attached hardware expansion module. But when I select the Profibus expansion module as DP slave and load the program to hardware it shows SF (system fault) error on the hardware. Without the selection of a DP slave, it does not assign a DP master to the expansion module. So, what could be the possible solution to configure hardware? Thanks, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/21/2023 07:08:46New subject after splitting |
|
6/24/2023 12:50 PM | |
Joined: 9/27/2006 Last visit: 10/3/2024 Posts: 12283 Rating: (2685) |
Hello 12re; In order for us to be able to hekp you, you need to provide better information. Your picture shows you are inserting a 7KM9300-0AB00-0AA0 Profibus expansion module, which has been replaced with the 7KM9300-0AB01-0AA0 and is now considered obsolete, as you mention. A 7KM9300-0AB00-0AA0 Profibus expansion module for the PAC3200 should still be available as a DP save if it is corretly integrated in your hardware configuration. Whch gsd file have you installed for this 7KM9300-0AB00-0AA0 module, there are 2 files available in this download for the module, which one did you choose to install? https://support.industry.siemens.com/cs/ca/en/view/27552047 When you selected the Profibus module in your Hardware Config Profibus network, which module did you choose, in which directory did you look? Most oftwn, Profibus slaves that are integrted through a gsd file have to be selected in the "Additional Field Devices" directory. Please examine section 6.4 of the following manual, an show us a screenshot of your own Profibus configuration. https://www.sahkonumerot.fi/6701100/doc/technicalinfodoc/ Hope this helps, |
Follow us on