1/11/2008 9:52 AM | |
Posts: 6 Rating:
|
hello how can we make a communication? with downloaded GSD file, was not work thank you |
1/11/2008 11:34 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi, I'm not a drive expert, but there is a handbook with the description of Profibus DP with the Sinamics S120 Control Units and additional system components & Drive Functions The S5 could couple with the IM 308C if the Sinamics S120 is NOT DPV1... I have checked both manuals but I couldn't find anything for communicating with SIMATIC S5 or what is needed as Protocol on Profibus, I see on some places that PROFIdrive might be the protocol... I think that is a Profibus DPV2 protocol... If it is, then it won't work... But please ask in the Product Conference of SIMAMICS if this is the matter. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/13/2008 11:42 PM | |
Joined: 9/1/2005 Last visit: 7/24/2024 Posts: 4103 Rating:
|
closed cause question posted twice. The second thread with the subject communication S5 with sinamics s 120 is published within the conference SINAMICS. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on