3/7/2020 3:11 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello Electrical designer; The first of the following FAQs will show you the step-by-step settings required to make a CPU 315-2DP a Profibus slave.The example uses a S7-400 as a Profibus master, and the data exchanged has been prepared for the requirements of that project, you will have to adapt with what you plan to exchange between your M-580 and your CPU 315-2DP slave. Notice that in the 2 CPUs (master and slave) the data table is symmetrical, but reversed: what is input to the master is and output from the slave, what is output from the master becomes an input to the slave. The second link holds the S7-300 gsd files; gsd files are text-based documents that are required in the Profibus configurator that you will use (I remember that Schneider used Sycon, this might no longer be the case with their newer models ..). Select the correct CPU, open the zip file and use the file with gse extension if you want English text; integrate it in your Profibus configurator, then you can setup a CPU 315-2DP as a Profibus slave in your configuration. How do you add a CPU as DP slave to the DP master system of a different CPU whereby the CPUs are configured in different STEP 7 projects? https://support.industry.siemens.com/cs/ww/en/view/19449428 PROFIBUS GSD files: SIMATIC https://support.industry.siemens.com/cs/ww/en/view/113652 This document discusses a similar issue, between a Schneider Modicon Premium as a master, with a S7-300 PLC as a slave over Profibus, it may shed more light on the subject. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 03/07/2020 16:09:43 |
|
This contribution was helpful to
1 thankful Users |
3/8/2020 7:28 PM | |
Posts: 5 Rating:
|
Hi Daniel Chartier,
I did configuration in S7300 Side as well as M580 side. For your Clear idea Earlier my S7-300 (CPU315-2DP- Profibus Slave) configured with S7 400 (Profibus Master) . Due to Process requirement new Configuration like S7 300-CPU 315-2DP (Profibus-Slave) & PRM (Profibus-Master) with M580 Controller. Curre New Configuration Changed as per the requirement, but now my CPU 315-2DP having System Fault and BF blinking. Other SidePRMshowingconfiguration FaultandSystem Fault. I want to know what is the Exact Data mapping need to be done in S7 300, so same Configuration I will be consider in the other side (3rdParty- PRM) . Please advice Thanks in Advance AttachmentSystem Configuration Details.zip (950 Downloads) |
Follow us on