3/5/2025 5:07 PM | |
Joined: 4/25/2015 Last visit: 8/22/2025 Posts: 114 Rating:
|
Dear all, I'm working with TIA V19 and have to operate a Confort panel V2 6AV2124-0UC02-0AX1. The panel has FW17.0.0.6 and TIA V19 propose 17.0.0.0 and ask me at download to downgrade to 17.0.0.0 I can't install the panel images because WinCC advanced V17 is mandatory to install the images. So, I tried to follow the instructions proposed in the forum and downloaded the image 17.0.0.0 but now I'm blocked without knowing what to do with it. Can anybody help me to downgrade it without installing V17. Best regards Claude ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/06/2025 00:21:39New subject after splitting |
|
3/6/2025 11:36 AM | |
Joined: 2/11/2015 Last visit: 9/9/2025 Posts: 512 Rating:
|
Hi claude_reckinger, Look into: https://support.industry.siemens.com/cs/ww/en/view/109778386 Do the steps indicated and copy the firmware inside your TIA v19. |
Last edited by: Moderator_Lan at: 03/06/2025 15:11:22link optimized |
|
This contribution was helpful to
1 thankful Users |
3/6/2025 12:07 PM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi I don't quite understand exactly what you mean. In this case, you can upload the V17.0.0 firmware version to the panel via Prosave but then you will need to upload the V17.0.0.0 image version to the TIA Portal V19 in order to upload to the panel. As the PIU does not seem to be available yet, you must perform this upload of the image versions as discussed in point 1.2. of the following link: "Image Downloads for SIMATIC HMI Operator Panels: Comfort / Mobile / Basic Panels" This method is the alternative to the PIU.
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
5/12/2025 4:05 PM |
|
Joined: 5/12/2025 Last visit: 5/13/2025 Posts: 1 Rating:
|
I need the procedure, my project is in tia portal 19 |
Follow us on